- Stratix device properties
What is CIP Sync
CIP Sync allows accurate real-time synchronization of devices and controllers connected over Common Industrial Protocol (CIP) networks that require time stamping, sequence of events recording, distributed motion control, and support for highly distributed applications requiring increased control coordination.
CIP Sync is based on the IEEE 1588 standard - Precision Time Protocol (PTP), which enables precise synchronization of clocks in measurement and control systems. The clocks communicate with each other over the EtherNet/IP communication network. PTP enables heterogeneous systems that include clocks of various inherent precision, resolution and stability to synchronize.
Provide Feedback