Calibration view parameters

Calibration view parameters

The
Calibration
view includes these parameters:
Parameter
Description
Channel
Shows the channel number to which this configuration applies.
Calibration Range
Shows the value currently configured for the channel. Values display according to the
Input Type
selected:
  • Current (mA)
  • RTD (ohms)
  • Thermocouple (mV)
  • Voltage (V)
Calibration Gain
Shows the calibration gain reported by the device.
Calibration Offset
Shows the offset in units (mA, ohms, mV or V) as reported by the device.
Last Calibration Date
Shows the last calibration date for the channel. The time and date listed here is based on the time on the computer running the application.
Calibration Status
Shows the status of the calibration per channel as the calibration occurs. Valid values include:
  • OK
  • Error
Start Calibration
Select to begin the calibration process.
Start Calibration
is enabled when the device is inhibited, online with the controller, and at least one channel is selected to start the calibration process.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal