CJ Channels view parameters
The
CJ Channels
view (5094-IY8) includes these parameters:Parameter | Description |
---|---|
Cold Junction Channel | Shows the channel numbers that can be configured. |
Disable Compensation | Determines whether cold junction compensation for the channel is disabled. If the checkbox is selected, the rest of the row is disabled. |
Sensor Offset | Sets a bias value, in degrees C, which is added equally to both cold junction temperatures. |
Remote Cold Junction Channel | Determines which channel to use as a remote termination for this channel.
|
Provide Feedback