Configure KPI

Configure KPI

After adding an asset or component, you need to configure KPIs. Perform the following steps to configure KPIs:
  1. After adding an asset or component, select the
    KPIs
    tab.
  2. Click [Add KPI].
    Add KPI
  3. In the
    Basic Details
    tab, set these parameters:
    • Sensor Name
      : Provide the sensor name.
    • Unit of Measure
      : Provide the unit of measure.
    • Data type
      : Provide the data type.
    • Asset Class
      : By default, it shows the asset class details.
    • Configuration Status
      : Select the status from the drop-down list.
  4. Click [Next].
    Basic Details
  5. In the
    Configure Equation
    tab, perform the following actions:
    • Equation Name
      : Select the equation name from the drop-down list.
    • Version
      : Select the version from the drop-down list.
    • Map the variables to the virtual sensors.
    • Click [Next].
      Configure Equation
  6. In the
    Configure KPI Limits
    tab, provide the values in the
    Alert Lower
    and
    Alert Upper
    .
    NOTE: Click the
    Auto-populate limits
    check box to add system-generated limits.
  7. Click [Add].
    Configure KPI Limits
    The KPI is added to the KPIs table and the "
    KPI was added under the asset successfully
    " message displays.
Perform the following steps to edit the KPI details:
  1. Select the required KPI check box from the KPI table.
  2. Click [Edit] and edit the required fields.
  3. Click [Save].
Perform the following steps to delete the KPI details:
  1. Select the required KPI check box from the KPI table.
  2. Click [Delete].
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal