KPI Configuration

KPI Configuration

Perform the following steps to configure KPI:
  1. Click
    Configuration
    >
    Dashboard setup
    from the menu bar.
  2. In the
    KPI Config
    tab, click the [+] icon in the
    Add KPI
    card.
    Select Add KPI
  3. In the
    Add Roll up KPI
    window, under
    KPI details
    , set these parameters:
    • KPI Name
      : Select the KPI name from the drop-down list.
    • Unit of Measure
      : Select the unit of measure from the drop-down list.
    • Aggregation Method
      : Select the aggregation method from the drop-down list.
    • Upper Limit
      : Provide the value.
    • Lower Limit
      : Provide the value.
    • Minimum Display Value
      : Provide the value.
    • Maximum Display Value
      : Provide the value.
      NOTE: By default, KPI is enabled. If you need you can disable it.
  4. In the
    Colors
    section, set these parameters:
    • Less than Lower Limit
      : Select the required color from the drop-down list.
    • Between Limits
      : Select the required color from the drop-down list.
    • Greater than Upper Limit
      : Select the required color from the drop-down list.
  5. Click [Add KPI].
    Add Roll up KPI
    The KPI is added to the
    KPI Config
    tab as a card.
    NOTE: Click the [] icon to edit the KPI details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal