Import Hierarchy

Import Hierarchy

Perform the following steps to import hierarchy:
  1. Click on the [] icon from the Enterprise in the hierarchy list and select [Import Hierarchy].
    Select Import Hierarchy
  2. In the
    Import Hierarchy
    window, click [Browse].
  3. In the pop-up window, select the required file and click [Open].
  4. You can preview the hierarchy details on the right side of the window and click [Import].
    Import Hierarchy window
    The "
    Hierarchy.xml imported successfully
    " message displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal