Underperforming Assets

Underperforming Assets

Perform the following steps to view the underperforming assets details:
  1. Click the [] icon from the menu bar.
  2. Select the required node from the hierarchy list.
  3. In the
    Underperforming Assets Tool
    window, set these parameters:
    • Asset Class
      : Select the asset class from the drop-down list.
    • KPI
      : By default, default KPIs are selected. If you want you can select the required KPI from the drop-down list.
    • Asset Count
      : Select the asset count from the drop-down list. Users can select the top 5, 10, 20, and 100.
  4. Click [Apply].
    NOTE: You can also filter the assets based on the date and the maximum time period allowed is one year.
    Now you can view all the assets in the table based on your selection. In the table, ranking, asset, asset class, and site columns are fixed and only the KPI column will move. The ranking is done based on the
    KPI multiplied value
    column.
    Underperforming assets
  5. Click the [] icon and select the
    Set as Default
    option to set the current filter option as default.
  6. Click the [] icon and select the
    Load Default
    option to filter the assets based on the default filter option.
  7. Click the [] icon and select the
    Download Result
    option to export the current table in Excel format.
    Set Default
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal