Add Region

Add Region

By default, Enterprise is added to the hierarchy list. The user can add a Region, Product, or Site under the Enterprise. Perform the following steps to add a Region:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Asset Setup
    .
  2. Click the
    Enterprise
    or
    Product
    node from the Hierarchy list.
  3. Click the [] icon and select
    Add Node
    .
  4. In the
    Add Node
    window, set these parameters:
    • Select item type
      : Select the Region radio button in the left pane.
    • Name
      : Provide the Region name.
    • Description
      : Provide a description of the Region.
    • Functional Location
      : Provide the location details.
      NOTE: Select the
      Auto Generate Functional Location
      checkbox to use the system-generated functional location.
    • Configuration Status
      : By default, Configuration Status is in Draft, and the user can select the required status from the drop-down list.
  5. Click
    Add
    .
    Add Region Window
    The "
    Region was added to hierarchy successfully
    " message is displayed.
  6. (Optional) In the
    Info
    tab, click
    Edit
    and perform the following actions:
    • Geographical Location
      : Provide the Geographical Location details.
    • Contact Details
      : Provide the Contact Details.
    • Remarks
      : Provide the Remarks details.
  7. Click
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.