Weighted Average Overview

Weighted Average Overview

Perform the following steps to view the weighted average overview:
NOTE:
  • Only Active nodes are displayed in the chart.
  • The [] icon indicates the weightage for the node is zero and it applies to its parent node till Enterprise. If the weightage of a node is zero, then the user will get notified at the following modules:
    1. Asset Setup
      : The notification is displayed at the node level, and click
      Define Weightage
      in the notification, the user is navigated to Dashboard Setup to define the weightage of the node.
    2. Dashboard
      : The notification is displayed at the parent level, and click
      Define Child Weightage
      in the notification, the user is navigated to Dashboard Setup to define the weightage of the child node.
  • The [] icon indicates the weightage is defined to a node.
  • This tab is disabled when the weighted average method is not selected for any of the three roll up KPIs.
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Dashboard Setup
    .
  2. Click the
    Weighted Average Overview
    tab and the Weighted Average Overview page is displayed.
    Weighted Average Overview
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.