Pre-Defined Formulas

Pre-Defined Formulas

Perform the following steps to view the pre-defined formulas:
  1. On the left navigation menu, drop-down the
    Configuration
    menu and click
    Formula Setup
    .
    The
    User defined Formulas
    tab is displayed.
  2. Click the
    Pre-Defined Formulas
    tab.
  3. Click on the required formula name to view the relevant details.
    View Pre-Defined Formula
    NOTE:
    The
    Utilized in app
    column is added to the existing table and it displays only Yes or No based on the association with KPIs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.