Add Favorites

Add Favorites

The user can add Favorites to any card at any level. The steps to add Favorites are similar for all levels of cards.
Perform the following steps to add Favorites to the
Region
card:
  1. Select the Enterprise node from the Hierarchy list.
  2. Click the [] icon on the required card and select
    Add to favorites
    .
    Add to Favorites
    "
    Card added to Favorites successfully
    " message is displayed. The Favorites icon [] is added to the selected card and the card is moved to the beginning of the summary section.
    Favorites Icon
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal