Underperforming Assets

Underperforming Asset

Perform the following steps to view the Underperforming Asset details:
  1. On the left navigation menu, click
    Underperforming Asset
    .
    The Underperforming Asset page is displayed.
  2. In the
    Underperforming Assets Tool
    window, set these parameters:
    • Asset Class
      : Select the required Asset Class from the drop-down list.
    • KPI
      : Select the required KPI from the drop-down list.
    • Asset Count
      : Select the required Asset Count (5, 10, 20, 100) from the drop-down list.
  3. Click
    Apply
    .
    NOTE: The user can filter the Assets based on the date and the maximum time period allowed is one year.
    All the Assets are displayed in the table based on your selection. In the table, Ranking, Asset, Asset Class, and Site columns are fixed and only the KPI columns are movable. The Ranking is done based on the KPI multiplied value column.
    Underperforming Assets
  4. Click the [] icon and select the
    Set as Default
    option to set the current filter option as default.
  5. Click the [] icon and select the
    Load Default
    option to filter the Assets based on the default filter option.
  6. Click the [] icon and select the
    Download Result
    option to export the current table in Excel format.
    Set Default Filter and Download Result
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal