Configure Automatic Renewals

Use the
Configure Automatic Renewals
page to accomplish the following tasks:
  • Enable or disable automatic renewals.
  • Specify the number of days between checks for automatic renewal of activations.
To configure Automatic Renewals:
  1. Access the
    Configure Automatic Renewals
    page by selecting the
    Advanced
    tab and choosing
    Configure Automatic Renewals
    .
  2. Verify that
    Automatic Renewals Enabled
    is selected. Automatic Renewals is enabled by default.
  3. Enter a number from 1 to 10 for the
    Time in days between check for renewable activations
    .
  4. Select
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.