Deny access to a firm code
Configure
CodeMeter
options to deny access to all computers to all activations of a specific firm code, such as 102389 or 6000458.- Keep these considerations in mind when configuringCodeMeteroptions:
- Only activations that are currently on the server can be configured.
- Changing the access rules might require a refresh of theCodeMeterserver.
- To configure a computer to be a CodeMeter server, select theRun Network Serverbox on theAdvanced > Configure CodeMeterpage.
To deny access to all computers to all activations of a specific firm code:
- OpenFactoryTalk Activation Manageron the server computer and click theAdvancedtab.
- ClickConfigure.CodeMeter
- ClickWeb Adminto open theCodeMeterWebAdmin utility.Tip:In theCodeMeterWebAdmin utility, click the help
icon for more information on settings and parameters.
- In theModebox, selectAdvanced.
- In theAdvanced Mode Configurationbox, underSpecific access rules, clickAdd new Firm Codeto open theAdd Firm Codebox.
- Select the firm code to configure and clickAdd. The firm code is added underSpecific access rules.
- For the default action, selectDeny. All computers are denied access to use the specific Rockwell Automation software activations of the firm code. However, computers are automatically allowed access to localhost (the server computer).
Provide Feedback