Bind an activation to an Ethernet MAC ID
Use the following procedure to bind an activation to an Ethernet MAC ID manually.
To bind an activation to an Ethernet MAC ID:
- On theFactoryTalk Activation Managerpage, clickManage Activations.
- ClickGet New Activations.
- Enter the serial number and product key for the product that you want to activate and clickValidate Activation.
- (optional) For each product in theValidate Activationtable, theProduct Versioncolumn displays the earliest version of the product available. Use this default value or select a different version.
- To download more than one copy of the activation, edit the value in the# to Downloadcell.
- Click in theBindingfield and enter the 12-character MAC ID as one contiguous string. Do not include spaces or colon (:) separators. For example: 0123456789AB.
- ClickDownload Activation.
- After the activations have downloaded, clickPrintto save a copy of the activation information for your records.
Provide Feedback