G - Z

G - Z

node-locked activation
An activation that is locked to a specific piece of computer hardware and is used only on the computer to which it is locked. Examples of computer hardware used for node-locked activation include an Ethernet card, a hard disk drive, or a dongle. Node-locked activation is not supported by all products. See your product documentation for information on what types of activation it supports.
rehost (an activation)
Rehosting an activation provides a way of moving an activation file from one computer or device to another. Rehosting an activation file deactivates the file on the computer that is hosting it and then creates a rehost code that Rockwell Technical Support staff can use to generate a new activation file for use on another computer.
rehost code
A code generated by FactoryTalk Activation Manager when you rehost an activation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal