Add a server to the search path
The search path identifies the locations that clients can use to obtain activations. Use the following procedure to add an activation server to the
Find Available Activations
search path.To add a server to the search path:
- Click theManage Activationstab.
- On theFind Available Activationspage, click theUpdate Activation Search Pathlink.
- ClickAdd Server. A new line is added in thePath to Activationslist.
- Type the path to the server or click theBrowsebutton
to open the
Browse for Serverdialog box to navigate to and select the server using the network tree. After locating the server in theBrowse for Serverdialog box, clickOKto return to theUpdate Activation Search Pathdialog box. - Select the checkbox next to the server, and clickSave.
- ClickRefresh Activationsto see the changes in the search path list.
Provide Feedback