Change the search path order of servers

Change the search path order of servers

When you run
Rockwell Automation
software,
FactoryTalk Activation
first searches for an activation on the activation server at the top of the
Path to Activations
list. If the activation file is not available on that server, the system searches the next activation server in the list. Use the following procedure to change the order of the search paths.
To change the search path order:
  1. Click the
    Manage Activations
    tab.
  2. Click the
    Update Activation Search Path
    link.
  3. Click a server path that you want to move up or down in the list.
  4. Click
    Up
    or
    Down
    to reposition the search path in the table.
  5. When all server paths are properly ordered, click
    Save
    .
  6. Click
    Refresh Activations
    to see the changes in the search path list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal