Remove a server from the search path

Remove a server from the search path

Remove an activation server from the search path to help prevent client computers from attempting to connect to a server that is no longer available. To remove an activation server from the
Available Activations
search path, use the following procedure. The default path for local activations is always displayed and cannot be removed from the list of activation locations.
To remove a server from the search path:
  1. Click
    Manage Activations
    >
    Find Available Activations
    .
  2. Click
    Update Activation Search Path
    .
  3. Select the activation server to be removed. The row is highlighted.
  4. Click
    Delete
    . The
    Confirm Delete
    dialog box is displayed. Click
    Yes
    to delete the activation server from the search path.
  5. Click
    Save
    .
  6. Click
    Refresh Activations
    to see the changes in the search path list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.