ConfigWSCert

ConfigWSCert

Use the
ConfigWSCert
command to configure the certificate file and password that will be used to secure the connection between clients and the
FactoryTalk Activation
Websocket Service.
These options are required:
  • '-c, --certfile': specifies the certificate filename and path.
  • '-p, --certpassword': specifies the password.
Usage: configwscert [options]
This table describes the command options.
Option
Description
-v|--verbose
Use this option to turn on trace messaging.
-c|--certfile
Specifies the
FactoryTalk Activation
Websocket Service certificate filename and path.
-p|--certpassword
Specifies the
FactoryTalk Activation
Websocket Service password.
-r|--restart
Either enable and start the service or restart the service.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal