ConfigWSPort

Use the
ConfigWSPort
command to configure the port number that will be listened on by the
FactoryTalk Activation
Websocket Service.
The '-p, --port' option, which specifies a port number, is required.
Usage: configwsport [options]
This table describes the command options.
Option
Description
-v|--verbose
Use this option to turn on trace messaging.
-p|--port
Specifies the port number that will be listened on by the
FactoryTalk Activation
Websocket Service.
-r|--restart
Either enable and start the service or restart the service.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.