ConfirmBorrow

Use the
confirmBorrow
command on the source computer to complete a borrow operation without a server connection. Requires the transport data file created from the
selectBorrowDestination
,
selectBorrowSource
, and
importBorrow
commands.
IMPORTANT: A disconnected borrow operation is only supported by CodeMeter activations.
These options are required:
  • '-d, --disconnected'
Usage: confirmBorrow [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the data transport file.
Example: '-d:C:\Users\jdoe\Documents\BorrowByFileData.xml'
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.