Get

Use the
get
command to download an activation.
These options are required:
  • '-sn, --serialnumber'
  • '-pk, --productkey'
These are optional:
  • '-b, --binding',
  • '-l, --locationcomputer,'
  • '-q, --quantity',
  • '-pv, --productversion'
These options can be included multiple times:
  • '-sn, --serialnumber',
  • '-pk, --productkey',
  • '-q, --quantity',
  • '-pv, --productversion'
    NOTE:
    Notes:
    • The number of -pk options included must match the number of -sn options.
    • If more than one -q option is included, it must match the number of -sn options.
    • If -pv options are included, they must match the number of -sn options.
    • The multiple options are order dependent. The first -sn value is used with the first -pk, -q, and -pv values. The second -sn value is used with the second -pk, -q, and -pv values, and so on.
Usage: get [options]
This table describes the command options.
Option
Description
-v|--verbose
Turns on trace messaging.
-d|--disconnected
Use this required option to support disconnected workflows (get, rehost, and renew). You can specify a file spec for the data transport file. If you do not specify the file spec, a default file spec is used.
Example: '-d:C:\Temp\TransportFile.xml'
Note: '-d C:\Temp\TransportFile.xml' results in a parsing error. You must insert either ':' or '=' when specifying the data transport file.
Note: The file spec must be for an xml file and therefore have an .xml file extension.
-sn|--serialnumber
Required: The 10-character, alpha-numeric serial number provided in the Activation certificate.
You can include multiple serial numbers but you must also include the same number of -pk options.
Example: '-sn 5555566778'
-pk|--productkey
Required: The 10-character, alpha-numeric product key, with optional '-' in the middle, provided in the Activation certificate.
You can include multiple product keys but the number must match the number of -sn options.
Example: '-pk YG7VM-T4WKU'
-b|--binding
Optional: The binding identifier.
Example: '-b 3-3519398' Example:'<computername>:130-3618734
where <computername> is the name of the computer. You might need to include the computer name when specifying remote bindings for disconnected get workflows.
-l|--locationcomputer
Optional: This is a special binding qualifier that only applies when you specify an FNP/Flexera dongle binding. When you include this option, the .lic file is stored on the computer.
If -l/--locationcomputer is not specified, the .lic file is stored on the FNP/Flexera dongle.
Example: '-b FLEXID=9-41e14904 -l'
-q|--quantity
Optional: The install count/quantity to be downloaded. If you do not specify a quantity, an install quantity of 1 is used.
You can include multiple quantities but the number must match the number of -sn options.
Example: '-q 5'
If one -q is included, its value will be used for all -sn options included.
-pv|--productversion
Optional: The product version. If you do not specify a version, the latest product version of the activation is used.
You can include multiple product version options but the number must match the number of -sn options.
Example: '-pv 32.00.00'
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.