importActivations

ImportActivations

Use the
importActivations
command to import activations from the specified directory.
This option is required:
'-i, --importdirectory'
Usage: importActivations [options]
This table describes the command options.
Option
Description
-i|--importdirectory
Use this required option to specify the directory where the activation files (*.lic and/or *.WibuCmRaU) are imported from.
Example: '-i C:\Users\Public\Desktop'
Example: '-i D:\Activations\<computername>' where <computername> is name of a computer, such as WIN-VPLD4SB9KWG.
-v|--verbose
Use this option to turn on trace messaging.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal