ImportBorrow

Use the
importBorrow
command on the destination computer to import a transport data file created using
selectBorrowDestination
and
selectBorrowSource
. This command and
confirmBorrow
complete a borrow operation without a server connection.
IMPORTANT: A disconnected borrow operation is only supported by CodeMeter activations.
These options are required:
  • '-d,--disconnected'
Usage: importBorrow [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the data transport file.
Example: '-d:C:\Users\jdoe\Documents\BorrowByFileData.xml'
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.