ImportRehost

Use the
importRehost
command to collect the rehost data to import from the specified transport data file and import it.
This is the third step in the disconnected rehost workflow. Run this command on the computer where the activation is being returned. The
general --disconnected
option specifying the transport data file is required. This command is the import process that removes the activation from the computer.
Usage: importRehost [options]
This table describes the command options.
Option
Description
-d|--disconnected
Use this required option to support disconnected workflows (get, rehost, and renew). You can specify a file spec for the data transport file. If you do not specify the file spec, a default file spec is used.
Example: '-d:C:\Temp\TransportFile.xml'
Note: '-d C:\Temp\TransportFile.xml' results in a parsing error. You must insert either ':' or '=' when specifying the data transport file.
Note: The file spec must be for an xml file and therefore have an .xml file extension.
-v|--verbose
Use this option to turn on trace messaging.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.