Renew
Use the
renew
command to renew an activation. Only activations whose serial number has been renewed in the Rockwell Automation
subscription portal are renewable. This option is required:
- '-sn, --serialnumber'
This parameter is optional:
- '-b, --binding'
These options can be included multiple times:
- 'sn, --serialnumber'
Usage: renew [options]
This table describes the command options.
Option | Description |
---|---|
-v|--verbose | Turns on trace messaging. |
-sn|--serialnumber | Required: The 10-character, alpha-numeric serial number provided in the Activation certificate. You can include multiple serial numbers. Example: '-sn 5555566778' |
-b|--binding | Optional: The binding identifier. Use the GetBindings command to determine possible binding indentifiers.Example: '-b 130-2526232760' |
-?|-h|--help | Show help information. |
Provide Feedback