searchpath

Searchpath

Use the
searchpath
command to read or modify the
FactoryTalk Activation
server search path with one of the command options.
Usage: searchpath [options]
This table describes the command options.
Option
Description
-v|--verbose
Use this option to turn on trace messaging.
-g|--get
Displays the current Activation server search path.
Example: 'searchpath -g'
-a|--add
Add a server path to the Activaton server search path.
Specify a server path to add.
Example: 'searchpath -a 10.10.10.10' or 'searchpath -a Computer100
-r|--remove
Removes a server path from the Activaton server search path. Specify a server path to remove.
Example: 'searchpath -r 10.10.10.10' or 'searchpath -r Computer100.
-?|-h|--help
Show help information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal