SelectBorrowSource

SelectBorrowSource

Use the
selectBorrowSource
command on the source computer to update a transport data file created by
selectBorrowDestination
to contain information about the source binding. The resulting file can be used with the
importBorrow
and
confirmBorrow
commands to perform a borrow operation without a server connection.
IMPORTANT: A disconnected borrow operation is only supported by CodeMeter activations.
These options are required:
  • '-d:
    filepath
    '
  • '-sb, --sourcebinding'
  • '-fn, --featurename'
  • '-fv, --featureversion'
  • '-bt, --borrowterm'
Usage: selectBorrowSource [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the data transport file.
Example: '-d:C:\Users\jdoe\Documents\BorrowByFileData.xml'
-sb|--sourcebinding
The source binding identifier. This is the binding where the activation will be borrowed from.
Example:'-sb 130-3618734'
In this example, the value is the CodeMeter container id/mask-serial number used when borrowing a CodeMeter activation.
-fn|--featurename
The feature name of the activation to borrow.
Example: 'RS5K_600.EXE'
-fv|--featureversion
The feature version of the activation to borrow.
Example: '1.00'
-bt|--borrowterm
The period of time the specified activation will be borrowed for, in the form <number of days>:<number of hours>.
Example: '90:0' or '0:8'
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal