SelectReturnSource

SelectReturnSource

Use the
selectReturnSource
command on the destination computer to create a transport data file containing information about the activation to be returned. The resulting file can be used with the
writeReturnUpdate
,
importReturn
, and
confirmReturn
commands to perform a return operation without a server connection.
IMPORTANT: A disconnected return operation is only supported by CodeMeter activations.
These options are required:
  • '-d, --disconnected'
  • '-sb, --sourcebinding'
  • '-db, --destinationbinding'
  • '-fn, --featurename'
Usage: selectReturnSource [options]
This table describes the command options.
Option
Description
-d|--disconnected
The filepath for the data transport file.
Example: '-d:C:\Users\jdoe\Documents\ReturnByFileData.xml'
-sb|--sourcebinding
The source binding identifier. This is the binding where the activation will be returned.
Example:'-sb 130-3618734'
In this example, the value is the CodeMeter container id/mask-serial number used when returning a CodeMeter activation.
-db|--destinationbinding
The destination binding identifier. This is the binding where the activation will be borrowed to.
Example:'-db 130-3618734'
In this example, the value is the CodeMeter container id/mask-serial number used when borrowing a CodeMeter activation.
-fn|--featurename
The feature name of the activation to return.
Example: 'RS5K_600.EXE'
-?|-h|--help
Show help information.
-v|--verbose
Use this option to turn on trace messaging.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.