Inaccurate display of activation expirations
Possible cause and solution:
- CodeMeter activations expire at a specific hour, minute, second. In FactoryTalk Activation Manager, the CodeMeter activation expiration time is at the beginning of the day. Depending on the time of day, theFind Availablepage may show a CodeMeter activation as available even though the activation expired and is not usable.To view the CodeMeter activation expiration times, inCodeMeter Web Admin, selectContainer > Licenses.TheFind Availablepage and CodeMeter activations are consistent the beginning of day after the expiration date.TIP: FlexNet Publisher activation expiration time is at the end of the day.
Provide Feedback