A computer is consuming too many of the activations on the server
Possible cause and solution:
- By default, capacity activations are granted on a first come first served basis.If one computer is requesting an excessive number of activations, edit the Options file to set a MAX number of licenses for that host computer by adding a line in the following syntax:MAX [count] [featurekey] HOST [name]For example, if you wanted to keep the computer "SharedOps" from obtaining more than three activations forRSLinxyou would use the following line:MAX 3 RSLINX.EXE HOST SharedOps
Provide Feedback