Activation checkout is denied
Possible cause and solution:
- All available activations are checked out.Wait until an activation is returned or contactRockwell Automationtechnical support to purchase additional activations.
- The activation file was modified.Rehost the activation file. Modified activations files are no longer valid. In these instances, get a new activation.
- The activation file contains an invalid license.Renew the activation file. If the license is invalid, a new license file must be granted from the activation server.
- The options file restricts access to activations.Update the options file to enable the required access.
- The activation is not available on the server providing activations.Update the Path to Activations to include the activation server that is hosting the activation needed.TIP: Additional information about denied activations may be available in the activation server log file.
Provide Feedback