Startup time is excessive

Possible cause and solution:
  • Network latency is impacting performance of the activation server.
    The Microsoft Loopback Adapter can affect local check in and check out of concurrent activations. Review the
    Microsoft
    hotfix 979612, which can improve TCP loopback latency and UDP latency in Windows Server 2008, Windows Server 2008 R2, Windows Vista, and Windows 7 to see if it applies to your system.
  • A computer listed in the
    Path to Activations
    is not accessible.
    From the
    Home
    page, click
    Manage Activations > Find available activations
    , and make sure each path in
    Path to Activations
    is correct. Also, remove any computer from the list that is no longer being used to provide activations and make sure that the order of the locations is optimal for providing activations without delays. Click
    Up
    or
    Down
    to reorder the activation paths.
  • The activation server is not running.
    Click
    Advanced >Refresh This Server.
    If the
    Server state
    is
    Stopped
    , click
    Refresh.
  • Network connection type slows down activation time when using virtual machine (VM) images and
    CodeMeter
    activations.
    Configure the virtual machine to use a bridged network connection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.