Activations not always available on a single computer

Possible cause and solution:
  • The activation is locked to a virtual network adapter, such as a virtual private network (VPN) or virtual machine or is locked to a device that is currently not available, such as a network adapter, docking station, or a network adapter on a laptop that automatically powers down when not in use.
    Rehost the activation. Get a new activation and lock it to the bindings of devices that are always available, such as hard disk drive serial numbers or Ethernet network adapters.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.