Cannot retrieve a binding from a dongle

Cannot retrieve a binding from a dongle

Possible cause and solution:
  • The dongle driver is not installed.
    Install the dongle driver.
  • The dongle drive is out of date.
    Check for updates to the dongle driver. If updates are found, install them and then try to retrieve the binding again.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal