FactoryTalk Activation Manager firewall ports and rules

Firewall ports and rules

Firewall rules allow a computer to send or receive traffic from programs, system services, other computers, or computer users.
FactoryTalk Activation Manager
uses the following Transmission Control Protocol (TCP) ports and rules.
Program
Ports
Rules
lmgrd.exe
,
Flexera Software
license daemon
One TCP port from 27000 to 27009.
Allow inbound traffic from one of these ports. The default is 27000. Non-default ports must be set in each license file.
FTActivationWebsocketService.exe
TCP port 27100.
Allow inbound and outbound traffic.
flexsvr.exe
,
Rockwell Automation
vendor daemon
One other TCP port, negotiated.
Allow inbound and outbound connections from one additional TCP port that will be negotiated at runtime.
codemeter.exe
, CodeMeter runtime server
TCP and UDP port 22350.
Allow all inbound and outbound connections from TCP and UDP port 22350.
Note:
You must also provide Internet access to cmtime.codemeter.com, cmtime.codemeter.us, or cmtime.codemeter.de as configured in the CodeMeter Web Admin/Configuration/Advanced/CodeMeter Time Server. This access is required due to the CodeMeter requirement for an independent time source from the computer’s system time.
For
Windows
Firewall,
FactoryTalk Activation Manager
automatically adds exceptions for
lmgrd.exe
and
flexsvr.exe
during installation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.