How FactoryTalk Activation works

How FactoryTalk Activation works

FactoryTalk Activation
works by binding the license for a
Rockwell Automation
software product to a specific device, such as a dongle, Ethernet address for a computer, or hard disk drive so that it can be run in a production environment. Once a license is bound, the product is activated. Without activation, some
Rockwell Automation
software products will not run, some will run with diminished functionality, and others will run for a limited time and then shut down with or without warning.
A system-generated signature that is based on machine-specific information that you provide when installing the software helps protect the activation. If the signature is tampered with, damaged, or deleted, the software will not function.
IMPORTANT: If an activation becomes corrupted, you must rehost the activation to rebind the license with the device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal