Elasticsearch Logs
The Elasticsearch Logs are enabled by default and are available in the path specified while installing Elasticsearch:
<<Elasticsearch Installation Directory>> ProgramData>Elastic>Elasticsearch>logs
TIP:
Unhide the hidden files. In the View menu, select the [Hidden items] checkbox. The hidden files display.
Hidden Files
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/adv-install-windows/troubleshooting/unhide.png/_jcr_content/renditions/original)
Elasticsearch Log
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/adv-install-windows/troubleshooting/010.png/_jcr_content/renditions/original)
Provide Feedback