Windows Event Logs

Windows Event Logs

Alternatively, you can also check the above logs using the Windows Event Viewer.
  1. In the Start menu search for “Event Viewer”. Click [Event Viewer] in the search results.
  2. Click [Windows Logs] and then click [Application].
  3. Double-click on the desired event. The Event Properties dialog displays.
    Windows Event Logs
    Details- Friendly View
    Details- XML View
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal