Configure Other Components

Configure Other Components

  1. Go to backup folder and copy the
    dataimporte.properties
    file and go to the new dataimporter directory and replace the existing
    dataimporte.properties
    file with the copied file. Path: %NEW_DATAVIEW_HOME%\
    FTADataView\dataimporter
  2. Go to backup folder and copy the
    application.properties
    file and go to new dataview directory and replace the existing
    application.properties
    file with the copied file. Path: %NEW_DATAVIEW_HOME%\
    FTADataView\dataview
  3. Start the following services:
    • FTAnalyticsDataImporter
    • FTAnalyticsDataView
  4. Verify successful installation. Verification Steps (Application Installation)Refer to Chapter 6, “Verification Steps (Application Installation)”.
  5. Open PgAdmin4 and verify “database product info table” as shown in the following image:
    Install Complete
  6. In the new web browser window, go to the DataView application using the DataView URL:
    https://<FQDN-hostname>/dataview
    This Application login page displays.
  7. Login as a DataView Admin User. The Admin console page displays.
    DataView Admin Console
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.