Database - MSSQL Connector

Database - MSSQL Connector

Perform the following steps to configure the MSSQL Connection:
  1. Click the Connection tab.
  2. Click [Add Connection].
  3. Select the MSSQL connection from the Connections List.
    Create Connection
  4. Define the following details:
    • Connection Name
      : Provide the Connection name.
    • Host Name (IP Address)
      : Provide the host system IP Address for the database instance.
      NOTE:
      For the sections, FQDN-hostname, if the database is installed on the same machine where the platform is installed, then localhost can be used.
    • Port
      : This is the listener port for the database. The port number varies based on database type (e.g. 1433 for SQLServer).
    • DB Name
      : Provide Database name.
    • User Name
      : User Name created by database Admin User.
      NOTE:
      User Name is case sensitive.
    • Password
      : Password created by database Admin User.
    • Folder Name
      : Select the folder name to save the Connection in the folder.
      Test Connection - Disabled Windows Auth
  5. Enable Windows Authentication
    NOTE:
    If the User enables the Windows Auth check-box, the User Name and Password are not required. To enable windows authentication steps refer to “Enable Windows Authentication” section.
    • Connection Name
      : Provide the Connection name.
    • Host Name (IP Address)
      : Provide the host system IP Address for the database instance.
      NOTE:
      For the sections, FQDN-hostname, if the database is installed on the same machine where the platform is installed, then localhost can be used.
    • Port
      : This is the listener port for the database. The port number varies based on database type (e.g. 1433 for SQLServer).
    • DB Name
      : Provide Database name.
    • User Name
      : Not Required.
    • Password
      : Not Required.
    • Folder Name
      : Select the folder name to save the Connection in the folder.
    Test Connection - Enable Windows Auth
  6. Click [Test Connection]. The “
    Test connection successful
    ” message displays.
  7. Click [Add] to create a connection “
    Connection saved successful
    ” message displays. The created connection will be saved in the folder.
    Test Connection
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal