Flat Files - CSV Connector

Flat Files - CSV Connector

Perform the following steps to configure the CSV Connection:
  1. Click the Connection tab.
  2. Click [Add Connection].
  3. Select the CSV connection from the Flat Files drop-down list.
    Create Connection
  4. Define the following details:
    • Connection Name
      : Provide the Connection name.
    • Click [Browse] and select a .csv file.
      NOTE:
      The size of the .csv file should not exceed 30MB.
    • Folder Name
      : Select the folder name to save the Connection in the folder.
      Unsupported Special Characters
      ->
      <
      >
      ,(As CSV is comma separated, so it considers as new field)
  5. Click [Verify CSV]. The “
    CSV verified successfully
    ” message displays.
    Test Connection
  6. Click [Add] to create a connection “
    Connection saved successful
    ” message displays. The created connection will be saved in the folder.
    Save Connection
  7. Select the connection the connection details displays.
    Connection Details
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.