Plant Manager Template
Perform the following steps to create a Storyboard with Plant Manager (FactoryTalk Metrics) template:
- Click [Add Content].
- Select the Content type as Storyboard.
- Select the Plant Manager Template from the Select a Template section.NOTE:Ensure that the FactoryTalk Metric Connection is already created.
- Navigate to the desired folder where the connections are saved.
- Select the FactoryTalk Metric Connection from the folder.
- Click [Add Content].NOTE:User can click [] to navigate to previous page.The Save Storyboard dialog displays.
- Provide the following details to enable the Save option:
- Content Name:Provide the Storyboard Name.
- Select Source Time Zone:Select the Source Time Zone from the drop-down list.
- Select folder for Content:Select the folder for Storyboard to be saved.
- Navigate to Content:Select the Content that the User will be able to navigate to. This will cause an association from the current Storyboard to the selected Content. Click the arrows in the bottom right corner to navigate to the linked Content.
- Click [Save].The "Storyboard created successfully" message displays.
- Use the vertical scroll bar to view the different charts in the Storyboard and horizontal scroll bar to view other columns in the data table.The default Semi Circle Gauge chart color changes based on the Y-Axis column value:Red0 to 30Yellow31 to 70Green70 to 100The saved Storyboard displays in the Storyboards section on the home page.
Provide Feedback