DataView License Behavior

DataView License Behavior

  • At Server Startup - Activations are obtained from the activation server.
  • Activations are refreshed continuously with Activation Manager.
  • User Messaging: Grace Period and Expiry message is shown as a red banner on bottom of the page. This message will be displayed in all screens for all types of Users.
  • Displays Connectors and Templates based on the available License.
  • If the system is in grace due to multiple reasons, messages related to all the reasons will not be shown on banner at once.
    Storyboard License Error
  • After adding new license or updating the existing license, it is recommended to stop the following services:
    • FactoryTalk Activation Websocket
    • FactoryTalkAnalytics DataView services.
  • Then Start the following services:
    • FactoryTalk Activation Websocket
    • FactoryTalkAnalytics DataView services.
      Storyboard License Error
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.