Types of Licenses
- FT Activation Manager provides different types of licenses and license packs for DataView:There are six license types supported by DataView:
- FTA.DVIEW.SVR
- FTA.DVIEW.CONTENT
- FTA.DVIEW.DU
- FTA.DVIEW.VU
- FTA.DVIEW.FTMetrics
- FTA.DVIEW.FTAE
- FTA.DVIEW.CONNECT
- FTA.DVIEW.INFOPLATFORMIMPORTANT:Based on the type of Licenses, the different types of Connections will be displayed.
- FTA.DVIEW.SVR
- This Server license enables the User to access the DataView application.NOTE:Without this license, the User cannot access DataView application.
- FTA.DVIEW.CONTENT
- This license activates 50 Contents. Content license provides 50 Contents, where the count is based on Storyboards that are individually saved in the system.
- FTA.DVIEW.DU
- This license activates one DataView Design User.
- Design User license allows the User to connect to the data sources or create and edit the Storyboards.
- FTA.DVIEW.VU
- This license activates one DataView View User.
- View User license allows the User to access existing content and interact with it by drilling down into the data, however they can not add dataset or create new Content.
- FTA.DVIEW.FTMetrics
- This license activates one FT Metrics Connector.
- FT Metrics license allows the User to create FT Metrics connection and create and save the Storyboards.
- User can create the number of Storyboards based on the available Content license.
- FTA.DVIEW.FTAE
- This license activates one FTAE Connector.
- FTAE license allows the User to create Alarms & Events connection and create and save the Storyboards.
- User can create the number of Storyboards based on the available Content license.
- FTA.DVIEW.CONNECT
- This license activates the Third-party Connectors i.e. MSSQL server and CSV file connectors.
- CONNECT license allows the User to create MSSQL and CSV connections and to create and save the Storyboards from these connections.
- User can create the number of Storyboards based on the available Content license.
- FTA.DVIEW.INFOPLATFORM
- This license activates the FactoryTalk Service Connectors i.e. FactoryTalk Service and FactoryTalk Edge Gateway connectors.
- INFOPLATFORM license allows the User to create FactoryTalk Service, FactoryTalk Edge Gateway connections and to create and save the Storyboards from these connections.
- User can create the number of Storyboards based on the available Content license.
Provide Feedback