Elasticsearch Remote Connection Configuration
Follow these steps for Elasticsearch remote connection configurations.
Prerequisite: |
Elasticsearch, JDK |
TIP:
Unhide the hidden files. In the View menu, select the [Hidden items] checkbox. The hidden files display.
Hidden Files
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/installer-windows/appendix/unhide.png/_jcr_content/renditions/original)
- Open the Windows Service management console and stop the Elasticsearch service.
- Open the Elasticsearchconfigfolder. The default config file location isC:\ProgramData\Elastic\Elasticsearch\config\elasticsearch.yml
- Open theelasticsearch.ymlfile in a text editor.Elasticsearch Config Folder
- Inelasticsearch.ymlfile, edit the cluster name and add additional parameters.
- Ensure that the cluster name is unique and is updated properly:cluster.name: FTAESCluster
- Add the following lines to the end of theelasticsearch.ymlfile and update the hostname:xpack.ml.enabled: false discovery.seed_hosts: ["<hostname>"] cluster.initial_master_nodes: ["<nodename>"]
TIP:If the user would like to add a backup file, add the following line to the end of theelasticsearch.ymlfile:path.repo: "C:\\work\\my_backup"User must also create a folder in the path specified above. This is an optional step and is not necessary. Also, if user needs to use IP address to access Elasticsearch, add the following line at the end of theelasticsearch.ymlfile:network.host: <hostname>Add Parameters - Save theelasticsearch.ymlfile once the changes have been made.
- Open the Windows Service management console.
- Start Elasticsearch service.Start Elasticsearch ServiceElasticsearch is now configured.NOTE:It is recommended to always use the HTTP port to access Elasticsearch in browser.
- Open a Web browser and type: http://<Hostname>:9200/?pretty.Verify Elasticsearch
Provide Feedback