Software Requirements

IMPORTANT:
Ensure that the user account used for installing DataView has administrator privileges.
It is recommended to enable long paths so that the directory path can be beyond the normal 255 character limit.
The following are the minimum software third-party requirements for installing DataView in the Windows environment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.