FT Activation Websocket Service Log
The FT Activation Websocket Service Logs are available in the following directory:
<<Installation_Directory>>Program Files (x86)>Rockwell Automation>FactoryTalk Activation Websocket Service>service.log
By default, Websocket Service log is not generated unless the error occurs.
If user wants to generate the log files in normal situation, user needs to change the log lever as required in
WebsocketService.dll.config
file.Example
: To view the Debug log change the loglevel value to <Debug>, as shown in the following image:FT Activation WebSocket Config file
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/installer-windows/log-files/013-1.png/_jcr_content/renditions/original)
FT Activation WebSocket Service Log
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/installer-windows/log-files/013.png/_jcr_content/renditions/original)
Provide Feedback