Create DataView User
Perform the following step to add DataView Users:
- Under the [Manage] section, select the [Users] menu and click [Add user].NOTE:DataView requires Users to have an associated email address. Additionally, DataView does not allow special characters (e.g., '-') in either the first name or last name fields. Choose a Username without special characters and provide an email address while creating the User.Add User
- Define the details for the DataView User. Click [Save].
- Provide the First Name of the User, assign the User to a Group, set a User Role and click [Update].
- From the [Groups] drop-down list, select the [DataView-Users] to assign the User to a Group.NOTE:Users should belong to a single Group. FactoryTalk Analytics applications do not support Users with both Admin and User Roles.
Add DataView UserThe User management screen displays.Save DataView User - Go to the [Credentials] tab and set an initial password for the User. The rest of the parameters are optional.IMPORTANT:Use a complex password as per the company policy.NOTE:The default password policy requires that passwords have a minimum length of 10 characters, at least one uppercase letter, one special character, and one lowercase letter.
- Click [Set Password] to save the password for the User.Initial Credentials DataView User
- The Set Password dialog displays, click [Set Password] to confirm and save the password for the User.
Provide Feedback